Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the IEC Contactors and Overload Relay be purchased together as a complete starter?
Issue:
Need to purchse the IEC contactor and overlod relay together.

Product Line:
LC1K, LC1D, LC1F Contactors. LR2K, LRD, LR3D, LR2D, LR9F Overload Relay

Environment:
IEC Contactors and Starters

Resolution:
Only the Tesys D can be purchased together, as an enclosed Tesys D starter. For the TeSys F and K lines the devices have to be purchased separately and assembled in the field.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings