Schneider Electric 3-wire RS-232 (p/n TBUM297859) and RS-485 (p/n TBUM297822) cables are used to connect an RS-232/RS-485 COM port (RJ45 connector) on the SCADAPack 300 and an RS-232/RS-485
SHORT HAUL DATA port (RJ45 connector) on Accutech Base Radio BR20 for Modbus communication.
BR20 SP300

SHORT HAUL DATA port (RJ45 connector) on Accutech Base Radio BR20 for Modbus communication.
BR20 SP300
Released for: Schneider Electric Canada