Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a DTM available for the BMXPRA0100 with M580?
Issue
Will be using an M580 to control an BMXPRA0100 module. Is there a DTM that can be added to the IO Scanner?

Product line
Unity Pro, Modicon M580, Control Expert

Resolution
Yes. Unity Pro V13.1 introduced the PRA DTM. It allows for a second instance of Unity Pro or Control Expert to be launched from the DTM where the BMXPRA0100 project can then be created and used as a template in the future.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings