How can we help you today?

ION9000 Meter Default IP Address, username, and password

Product Line
ION9000 Series

Environment
Web Server
Front Panel


Resolution
The username and password are defined by the meter’s security configuration; if standard security is enabled, the password is the same as the front display password.

See the ION9000 series meter factory default settings:
ParameterDefault value
Standard and advanced security display password0
Standard security mode username9000
Standard security web and ION Setup password0
Advanced security mode usernameUser1, User2, User3, etc.
IP Address169.254.0.10
Subnet Mask255.255.0.0
Gateway0.0.0.0
RS-485COM1 Unit ID: 100
COM2 Unit ID: 103
LanguageEnglish

Note: To help increase the security of your meter’s configuration and data, configure the meter’s username and passwords to be different from the default values.

For more information about the ION9000 series meter, please refer to the User Guide that can be downloaded at the link below:
ION9000 User Guide

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings