Video: What type of movement does a Homeline branch breaker have once mounted with and without the deadfront/cover installed?
Issue:
Demonstrating the small, acceptable movement of installed Homeline branch breakers both with and without the deadfront cover installed.]
Product Line:
Homeline Load Centers
Resolution:
Once a Homeline branch breaker is installed on the interior of a Homeline load center, there will be some small amount of movement of the breakers before the deadfront/cover gets installed. Then, as more branch breakers get installed next to each other, the movement will be reduced. Then once the deadfront/cover is installed, the movement of the branch breakers will be reduced even more.
Demonstrating the small, acceptable movement of installed Homeline branch breakers both with and without the deadfront cover installed.]
Product Line:
Homeline Load Centers
Resolution:
Once a Homeline branch breaker is installed on the interior of a Homeline load center, there will be some small amount of movement of the breakers before the deadfront/cover gets installed. Then, as more branch breakers get installed next to each other, the movement will be reduced. Then once the deadfront/cover is installed, the movement of the branch breakers will be reduced even more.
Released for: Schneider Electric Canada




Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.