Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to install the MPRPAF onto a PowerPacT R frame circuit breaker
Issue:
How to install the MPRPAF fixed padlock attachment for OFF position onto an R frame circuit breaker.

Product Line:
Circuit Breakers

Resolution:
The MPRPAF is a fixed padlock attachment which allows a PowerPacT R Frame circuit breaker to be padlocked in the OFF position. To install, watch the below video, or follow these steps.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Reference the picture below (typical shown for M, P and R circuit breakers).
  • Insert mounting screws provided through padlock attachment and into holes on circuit breaker accessory cover. 11 lb-in (1.2 N•m)
  • Move circuit breaker handle to OFF (O) position.
  • Move hinged portion of padlock attachment so tab prevents circuit breaker handle from moving.
  • Insert up to three padlocks shackle sizes: 3/16-5/16 in. (5-8 mm).

MPRPAF Pic

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings