Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: When a PowerPacT L frame breaker is installed in the L600AWK enclosures, what position does the enclosure operating handle move to when the breaker trips?
Issue:
Confirming tripped PowerPacT L frame L600AWK operator handle does not move.

Product Line:
PowerPact L-Frame Molded Case Circuit Breakers

Resolution:
When the L frame breaker installed in the L600AWK trips, the operating handle on the L600AWK will not move away from the 'ON' position. So the enclosure handle does NOT move to the center position or the OFF position.

See the video below for a demonstration:

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings