Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Adding device support for ION9000 and ION9810 in PME 8.x and PME 7.2.x
Issue
Newly released device type is missing in older version of Power Monitoring Expert software.

Product Line
Power Monitorig Expert 8.x
Power Monitorig Expert 7.2.x

Environment
Installer

Cause
New device type to be added to PME.

Resolution
Refer to the attachment for files and instructions.

Schneider Electric Canada

Attachment(s)
PME8x_ION9000_V2.0.0_Device_Updater_en_1.1.zip [1.92 MB]
PME72x_ION9000_V2.0.0_Device_Updater_en_1.1.zip [1.92 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings