Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the linkage to use with a VB-7313-0-4-11 2" 3W Valve and MP-371-600 actuator
Issue:
Is a linkage kit needed for a MP-371-600 actuator needed for use with a VB-7313-0-4-11 valve

Product Line:
Valves and Actuators

Environment:
Application

Cause:
Product Features

Resolution:
The AV-391 Linkage kit per attached Bulletin is needed for the Actuator to moun t to the VB-7313 3 Way Mixing valve

Schneider Electric Canada

Attachment(s)
MP300-MP400 F-15479.pdf [1.15 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings