Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the link cable part number for the M580 Hot Standby controllers?
The M580 Hot Standby controllers are shipped with empty SFP sockets. A choice needs to be made between a single mode fiber optic or an RJ45 copper SFP transceiver. These transceivers are purchased separately .

If the M580 HSBY link is to be fiber optic then the 490NAC0201 SFP transceiver is used. In the empty HSBY link SFP socket a 490NAC0201 is to be inserted each of the BMEH58xx40 redundant processors.

Unfortunately, We do not offer fiber cables for the M580 Hot Standby sync-link. The SFP interface (490NAC0201) uses a single mode fiber cable (9/125 nm) with LC/LC connectors on each end that can be purchased from any cable provider.

If the M580 HSBY link it to be Copper RJ45 Ethernet then the 490NAC0100 SFP transceiver is used. In the empty HSBY link SFP socket a 490NAC0100 is to be inserted each of the BMEH58xx40 redundant processors.

We provide a 5m Ethernet shielded twisted pair Cat5e straight copper cable that is UL compliant. That part number is 490NTW00005U.

You do not need to use that cable. You can use any shielded twisted pair Cat5e straight copper cable that is UL compliant as long as it is no longer than 100m.

There is no minimum length specified for this link as far as Hot Standby specifications go, but below are recommended copper wire minimum lengths.

If using a 100Base-T or below connection the recommended minimum length is 1 meter (3.28 ft). If using 1000Base-T, then there is no specified minimum connection.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings