Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the DC rating of the PowerPact B Frame Breaker?
Issue:
DC rating for the PowerPact B Frame breaker.

Product Line:
Molded Case Circuit Breaker

Resolution:
Updates on the PowerPact B Frame breaker have been released recently. There is no change to product fit and function. The faceplate label was modified to include the DC interrupt rating (UL, CSA, NOM). This modification includes 1P-4P PowerPact B MCCBs at D, G, and J interrupt ratings.
• 1P MCCB: 125 Vdc for D (10 kA), G (20 kA), and J (50 kA) interrupt ratings
• 2P-4P MCCB: 250 Vdc for D (10 kA), G (20 kA), and J (50 kA) interrupt ratings

MCCBs produced prior to October 2018 do not include DC ratings on faceplate label. The prior and current label may be used concurrently during a transition period through Q1 2019.

Powerpact B ratings labels

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings