Issue
ION8650 default communication parameters
Product Line
ION8650 series meter
Environment
Web Server
Front Panel
Cause
What are the default values the first time you connect to your meter.
Resolution
See the following ION8650 series meter default communication settings:
COM1 Setup:
| Protocol | ION |
| Baud Rate | 9600 |
| Unit ID | From Serial Number* |
| RS232 or RS485 | RS232 |
| Serial Port | 8N1 |
* The factory set Unit ID is based on the serial number of the meter. For example: Serial number: XXX-1009X263-XX is factory set to unit ID 9263
COM2 Setup:
| Protocol | ION |
| Baud Rate | 9600 |
| Unit ID | 101 |
COM3 Setup:
| Protocol | ION |
| Baud Rate | 9600 |
| Unit ID | 102 |
| Serial Port | 8N1 |
COM4 Setup:
| Protocol | ION |
| Baud Rate | 9600 |
| Unit ID | 103 |
| Serial Port | 8N1 |
Network Setup:
| IP Address | None* |
| Mask | None* |
| Gateway | None |
* To modify the NONE setting, press and hold the up arrow to enter edit mode.
Released for: Schneider Electric Canada