Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the ION6200 options card part numbers?
Issue
What are the ION6200 options card part numbers?

Product Line
ION6200

Environment
Part Numbers

Cause
Looking for the ION6200 series meter options card part numbers.

Resolution
See below the the available ION6200 series meter options cards:
Options cardPart Number
1 Standard MeasurementsP620KZ0A0N
2 Enhanced Package #1P620KZ0A0P
3 Enhanced Package #2P620KZ0A0R
4 Standard Measurements, two pulse outputsP620KZ0B0N
5 Enhanced Package #1, two pulse outputsP620KZ0B0P
6 Enhanced Package #2, two pulse outputsP620KZ0B0R
7 Standard Measurements, RS-485P620KA0A0N
8 Enhanced Package #1, RS-485P620KA0A0P
9 Enhanced Package #2, RS-485P620KA0A0R
10 Standard Measurements, two pulse outputs, RS-485P620KA0B0N
11 Enhanced Package #1, two pulse outputs, RS-485P620KA0B0P
12 Enhanced Package #2, two pulse outputs, RS-485P620KA0B0R

Please see the ION6200 Options Card retrofit instructions for how to install the Options Card:

Schneider Electric Canada

Attachment(s)
ION6200_Options_Card-70052-0144-05.pdf [187.81 KB]
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings