Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Installation and configuration of ENM 8.3.3

Issue
A user is installing and/or configuring Event Notification Module version 8.3.3 (ENM v8.3.3)

Production Line
Event Notification Module 8.3.3

Power Monitoring Expert 7.2

Power Monitoring Expert 8.x

Power Monitoring Expert 9.x

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024



Environment
ENM v8.3.3 documentation

Cause
It may be necessary to use related documentation when installing/troubleshooting/configuring the ENM v8.3.3 software

Resolution
Included FAQs for license activation, upgrading, installing, and configuring ENM v8.3.3

- License Activation (For PME 2020 and earlier)
FA225923

- Upgrading
FA252739

- ENM Installation
The ENM installer is included in the PME DVD (.iso)
Open the .iso (of Power Monitoring Expert)
Go to the folder: Event Notification Module
Go to the folder: Installer
Run: MainSetup.exe
Follow the instructions in the guide located in FA338107

- ENM Configuration
FA322882

- Related Documentation (primarily for v8.2 but greatly applicable to v8.3.3 as well)
FA235866

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings