Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will a 1000KVA Medium voltage Oil filled Nema 3R transformer 13.2KV to 480/277V including dead front on both sides, fit on a 75" x 60 slab ?
Issue:
What are the approximate dimensions for a 1000KVA 13,200V -480Y/277V  Oil Filled transformer with deadfronts ?

Product Line:
MV Oil Filled Tfmr

Environment:
Planning

Cause:
Product Features

Resolution:
The estimated dimensions of a 1000KVA Oil Filled Nema 3R Padmount transformer is 72.5”H x 88”W x 77.5”D.  An exact Dimension can be arrived at with a request for quote that can be provided by the Local SQ D /SE Sales Office Sales group and the Mfg Plant.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings