Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What copper cable is used to connect at BMXNRP020x to a BMxCRA312x0 module?

Issue
What kind of copper cable is used to connect  a BMXNRP020x fiber module to a BMxCRA312x0 Drop module?

Product line
M580, X80

Resolution
The BMXNRP020x to a BMxCRA312x0 connection is a standard RJ45 copper Ethernet connection. The maximum distance is less than 100m using shielded twisted 4-pair CAT5e or greater (10/100 Mbps) cable. (We do not recommend using twisted 2-pair CAT5e or CAT6 cables.)

Typically a customer will use anything that they already have available to them, at this link https://www.se.com/us/en/download/document/DIA6ED2140903EN/ you will find a catalog which includes a list of available ConneXium cables on page 24 (31). Any of the straight through will work.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings