Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H363DSWA, series F7 (may be shown as F07)?

Issue:
Deisgn repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The repair parts for the H363DSWA, series F7 (F07) are as follows. No other parts are available.
-Line Base Assembly - 4056775150 (1 required; arc suppressor not included)
-Load Base Assembly - 4056602850 (1 required)
-Line and Load Base Mounting Screws - 4020515101 (3 for line, 2 for load)
-Arc Suppressor Assembly - 4056635550 (1 required; obsolete, no longer available, replaced by ASKC603)
-Arc Suppressor Mounting Screw - 4020514501 (1 required)
-Lug Assembly - 4025101851 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056646950 (NOTE: mechanism/handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
-Mechanism/Handle Coupling - 4053922550
-Cover Interlock Defeat Coupling - 4056699750
-Lockplate Gasket - 4050322803 (2 required)
-Handle Assembly - 4056779850 (also recommend replacing lockplate gaskets)
-Lockplate - 4056681201 (also recommend replacing lockplate gaskets)
-Lockplate Mounting Screw 2194900001 (2 required)
-Rod/Linkage Assembly - 4056787150
-Receptacle - WRDK1034 (mounting screws included)
-Ground Lug - 4025101851 (3 required)
-Ground Lug Mounting Screws - 4020514801 (1 required) and 4020513503 (1 required)
-Fuse Pullers - FPK0610 (1 required)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings