Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the largest NF panel branch breaker available at 600V?
Issue:
What is the largest branch breaker available in an NF panel rated at 347/600V that can be added that does not require a sub-feed breaker kit.

Product Line:
Panel Boards

Resolution:
The largest 347/600V branch breaker available for an NF panel is a 100A rated EDB36100 that is rated 14 KAIC. This is also available at higher KAIC ratings such EGB36100 rated 18 KAIC and a EJB36100 that is rated 25 KAIC.
There was a 110A rated version that has been obsoleted and is no longer available.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings