How to change a PM5500 series meter to Client mode?
Product Line
PM5500
Environment
Front Panel
Webpages
ION Setup
Cause
What are the different ways to configure the PM5500 serial communications from server to gateway/ client mode?
Resolution
Setting up serial communication using the display:
Configuring serial settings using the webpages:
Configuring serial setting using ION Setup 3.0
PM5500
Environment
Front Panel
Webpages
ION Setup
Cause
What are the different ways to configure the PM5500 serial communications from server to gateway/ client mode?
Resolution
Setting up serial communication using the display:
- Navigate to Maint > Setup
- Enter the setup password (default is ’0’), then press OK
- Navigate to Comm > Serial
- Move the cursor to point to the ‘Mode’ parameter to modify, press Edit, press ‘+’ to change to Gateway, then press OK
- Press the up arrow to exit. Press Yes to save your changes
Configuring serial settings using the webpages:
- Login to the meter webpages using Product admin or Web admin credentials
- Click Settings > Serial Settings
- Modify the Mode setting by changing the value from ‘Server’ to ‘Gateway’
- Click Save changes
Configuring serial setting using ION Setup 3.0
- Connect to the meter in ION Setup
- In Setup Screens click on PM5500 series meter
- Navigate to RS-485 Comm Setup folder > Advanced Serial Settings
- Click Modbus Mode to highlight. Click Edit…
- In the dropdown menu for Select Modbus Mode select ‘Client Mode’. Click OK.
- Click Send to apply changes
Released for: Schneider Electric Canada
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.