Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PM5500 series meter display does not come on in a switchboard?
Issue
PM5500 series meter display does not come on in a switchboard?

Product Line
Switchboard
PM5500

Environment
Control Power
Display

Cause
The display for the PM5500 series meter is blank, the Operation/ Status LED is off and the display cable is connected properly.

Resolution
In a switchboard the gear comes pre-wired for the PM5500 series meter’s voltage, current and control power terminals. There is a disconnect switch in the gear that needs to be switched on in order for the PM5500 series meter to have control power for operation.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings