Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are combination arc fault breakers available for Stab-Lok panels?
Issue:
The current code requires combination AFI breakers to protect against parallel and series arcing. Is there a breaker to meet this requirement available for the Federal Pioneer Stab-Lok panels?

Product Lines:
Circuit Breakers

Resolution:
No, only AFI breakers are available for Stab-Lok panels. The only solution is to add a sub-panel (QO or Homeline) and add CAFI breakers.

NA15AFI, NA20AFI, NA15AFICP and NA20AFICP are offered as replacement breakers for existing AFI breakers as long as they do not requiring upgrading to current code requirements.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings