Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the ZBZ58 bellow be used with XB5AS86449B4 emergency stop operator?
Issue:
Bellows for XB5AS86449B4 illuminated emergency stop

Product Line:
Pushbutton and Operator Interface

Environment:
22MM Mushroom Operator

Resolution:
ZBZ58 is a Yellow bellows seal for a 22MM mushroom operator except for XB5AS86449B4.  The is no bellows or boot available for this type of operator.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings