Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the RIM module for use with Masterpact MTZ?
Issue:
RIM module for ZSI applications involving Masterpact MTZ

Product Line:
Circuit Breakers

Resolution:
The new RIM for ZSI applications involving the Masterpact MTZ is LV848892SP.  This module works with the Masterpact MTZ and older breakers as well.
See attached for instructions.

Note: LV848892SP will not work for AMS applications.  For AMS applications it will be necessary to convert to the ERMS arc-flash incident Energy Reduction Maintenance System.

Schneider Electric Canada

Attachment(s)
LV848892SP ZSI Interface NHA12883.pdf [3.68 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings