Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement trim screw for a Federal Pioneer Stablok panel?
Issue
What are the replacement speed screws for an FPE Stablok panel?

Product Line
Load Centres

Resolution
The replacement trim screws are part number S78B451. They are sold individually. This is a screw that probably cannot be found in the industry, it is a #10-7 Truss Comb. Screw Type "P" Dog Point, with a Thread Pitch of 0.1428", it is approximately 1.547" long

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings