Issue:
What are the lugs rated for on CH600SNC and CH600SN?
Product Line:
PTCCB-MCCBS, EARTH LEAK AND SWITCH
Resolution:
The CH600SN will accept (4) #1 - 750 kcmil Al/Cu wire PLUS (1) #4 - 300 kcmil Al/Cu service ground.
The CH600SNC will accept (2) #1 - 600 kcmil Cu and (2) #4 - 350 kcmil Cu PLUS (2) #6 - 250 kcmil Cu service ground.
What are the lugs rated for on CH600SNC and CH600SN?
Product Line:
PTCCB-MCCBS, EARTH LEAK AND SWITCH
Resolution:
The CH600SN will accept (4) #1 - 750 kcmil Al/Cu wire PLUS (1) #4 - 300 kcmil Al/Cu service ground.
The CH600SNC will accept (2) #1 - 600 kcmil Cu and (2) #4 - 350 kcmil Cu PLUS (2) #6 - 250 kcmil Cu service ground.
Released for: Schneider Electric Canada