Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PM55xx series firmware Version 2.7.4 and release notes
Issue
Looking for new firmware upgrade

Product Line
PM5500 series meter

Environment
Firmware Upgrade

Cause
Need to upgrade PM5500 series meter to the latest firmware version

Resolution
Release Notes: PM55xx firmware upgrade to address new and updated features for firmware version 2.7.4.

Updates: This version implements DNP3 protocol support over Ethernet and selection for the PM5563 for the PM5RD hardware version.

Note: This firmware update is intended for PowerLogic PM5560 and PM5563 meters.

Please see the following link for more information regarding PM5560 / PM5563 V2.7.4 Release

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings