Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How do you install and use the HOMELEC2PALA padlock attachment to lock 2p HOM electronic breakers in the ON or OFF position?
Issue:
Instructions and video on how to install and use the HOMELEC2PALA to lock 2p HOM electronic breakers in the ON or OFF position?

Product Line:
HOM Breakers

Resolution:
Remove the trim (if installed) of the panel. Place the padlock device tabs into the slots on the OFF end of the breaker. Press attachment flush to the breaker face and bend the locking prongs into the slots on the ON end of the breaker. To lock in the OFF position, turn the breaker OFF, slide the bail over the handle, and slide the padlock through the hole on the device. To lock in the ON position, turn the breaker ON, slide the bail under the handle, and slide the padlock through the hole on the device. For more information, see video below or the attached instruction bulletin.

Schneider Electric Canada

Attachment(s)
HOMELEC2PALA.pdf [470.2 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings