Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the Powerpact B Frame breaker fit into an old NH1B panelboard?
Issue:
Obsolete NH1B panelboards and replacement branch breakers
Product Line:
Obsolete circuit breaker panelboards
Environment:
Maintenance/replacement
Resolution:
The B frame breakers will not fit into the obsoleted NH1B panels and were never UL tested or approved for use in the NH1B interiors.
In addition, the NH1B mounting pan does not contain a tear drop shaped hole that is required for the B frame breaker mounting screw to fit into.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings