Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the driphood for EX45T65H Transformer?
Issue:
Which driphood can we use to convert to Nema 3R for a EX45T65H Transformer?

Product Line:
LV Transformer

Environment:
EX

Resolution:
7400WS18K is WeatherShield to convert  NEMA1 to NEMA 3R Outdoor.  7400DS18K Drip Shield to convert from NEMA 1 to NEMA 2 drip proof Indoor.

NEMA 2 prevents intrusion of dripping water from above like from a sprinkler head from splashing into the vent and onto the Transformer.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings