Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the QMB800T6 Class T fuse kit be used with a 800A QMB367W switch?
Issue:
Are there provisions for Class T fuses for a QMB367W switch?

Product Line:
QMB Panelboards

Environment:
Application

Cause:
Product features

Resolution:
TheQMB800T6 Class T fuse kit is available to be used with the QMB367MW Mains switch and QMB367W branch mounted switches. See attached bulletin for installation .

Schneider Electric Canada

Attachment(s)
QMB800T6 Instructions 40269-865-01.pdf [31.03 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings