Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I hot-swap the bus devices in TeSys Island?
Issue:
Does TeSys Island support hot-swap

Product Line:
Tesys Island

Environment:
Digital multifunctional load management solution

Resolution:
No, the island must be powered off to add or remove devices to the internal bus. However, thanks to fast device replacement if you are replacing only bus devices and keeping the bus coupler, the bus coupler will synchronize the new device to the appropriate firmware version and start working with it immediately upon power-up.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings