Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the ELM earth leakage module be used for ground fault alarm (without tripping)?
Issue:
Ground fault alarm with ELM

Product Line:
Circuit Breakers

Resolution:
No, the ELM cannot be used as an alarm only device.  Doing so will damage the ELM.
If the alarm only function is required, consider the Square D® Vigirex® ground fault relays.

NOTE: The companion circuit breaker must have an S29392 48 Vdc shunt trip accessory installed.
If shunt trip S29392 is not installed in the circuit breaker, it must be installed before placing into service.

Schneider Electric Canada

Attachment(s)
ELM Instr 48041-089-01 2010.pdf [6.17 MB]
Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings