Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between a blue vs black toggle on a Stab-lok NC015?
Issue:
What is the difference between a blue vs black toggle on the NC015 Stab-lok breakers?

Product line:
Circuit breakers

Resolution:
Older versions of the breaker had black handles and the shape of the handle tap was more square. Newer ones were colour coded to be blue, which was for the 15A devices. The handle shape was also changed to be more ergonomic. Ribs were added and the handle tab was slimmer and had a rounded end.
There is also a version of the newer shape handles which are black in colour. These are sold as bulk packaged.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings