Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why is my added DTM by EDS file not recognized by Control Expert for my imported Unity project?
Issue
After importing a Unity Pro project to Control Expert and adding the needed DTM by EDS file, the 'Dtm Audit Tool' is still not recognizing the DTM.

Product line
Control Expert, Unity Pro

Resolution
Make sure that 'New Naming convention' check box is unchecked when adding the EDS file. Towards the bottom of the window that is used to select the EDS file to be added there is a check box that is selected by default. This needs to be un-checked before bringing in the EDS file so that it conforms to the legacy Unity project naming convention.

If you have already added the DTM using the new naming convention, you will need to remove it. Below is a link on how to remove the EDS and steps for the entire process.

https://www.se.com/ww/en/faqs/FA288949/
  • OpenEcoStruxure
  • Remove EDS
  • Update HW Catalog
  • Close EcoStruxure
  • Open EcoStruxure
  • Add EDS w/ box unchecked for “New Naming Convention”
  • Update HW Catalog
  • Close EcoStruxure
  • Open EcoStruxure
Project now should be working/buildable

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings