Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a Powerpact 1200AF/1200AT P frame breaker with LSIG and Neutral CT be installed into a P1200 enclosure ?
Issue:
Can a Powerpact P frame LSIG breaker , with Neutral CT, be installed into a P1200X enclosure ?

Product:
Enclosed Circuit Breakers

Environment:
Application

Cause:
Product Features

Resolution:
The P1200 enclosures will be able to accept the breaker  with LSIG trip and Neutral CT up to 1200A as long as the breaker is 80% rated. If 100% rating is required, only P frame breakers 800A and below,can be used with LSIG and Neutral CT into the P1200X enclosures.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings