Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you replace the SDE switch on an electrically operated Powerpact P frame breaker?
Issue:
Can you replace the SDE switch on an electrically operated Powerpact P frame breaker or add a second one (SDE2)?

Product Line:
Circuit Breakers

Resolution:
No, the SDE switch is hard wired and cannot be removed or replaced. See attached photo.
There is no provision for adding a second SDE as there is with the Masterpact NW.

Schneider Electric Canada

Attachment(s)
P frame Motor operated SDE.jpg [3.21 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings