DISCLAIMER This sample program is intended to demonstrate one or more programming functions or methods and is presented as programming example only. Schneider Electric assumes no liability for the use or application of this example program or any portion thereof.
The below script example shows how to launch a GIS map focusing on a particular latitude and longitude. The latitude and the longitude are passed as mimic parameters in this example. Thus it is easy to scale this up by having various embedded instances of the same mimic with different values passed to the mimic parameters.
This is the source mimic:
Here is the script created in the source mimic:
The script is executed by clicking the Map With Params button located in the source mimic.
The 2 instances of the source mimic were embedded onto the main mimic. The mimic parameters were populated with the GIS location properties for either site:
The below script example shows how to launch a GIS map focusing on a particular latitude and longitude. The latitude and the longitude are passed as mimic parameters in this example. Thus it is easy to scale this up by having various embedded instances of the same mimic with different values passed to the mimic parameters.
This is the source mimic:
Here is the script created in the source mimic:
Sub OpenMap
Dim pLatitude, pLongitude
Set test = Mimic.Parameters
pLatitude = test.Point.Latitude
pLongitude = test.Point.Longitude
Mimic.OpenInset "SCX:////CGISMapSet/.My Map Set#zoom=12&Latitude=" & pLatitude & "&Longitude=" & pLongitude, 10, 10, 90, 90
End Sub The script is executed by clicking the Map With Params button located in the source mimic.
The 2 instances of the source mimic were embedded onto the main mimic. The mimic parameters were populated with the GIS location properties for either site:
Released for: Schneider Electric Canada