{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to generate a single value using sql and display it on a mimic in ClearSCADA?
Yes, this can be done using one of the following options:
  • An embedded list.
  • Run a SQL query in a Structured Text logic program and assign the result to an Internal Point.
  • Creating an ODBC Point that refers to an ODBC Connection built with internal ClearSCADA Database.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.