How can we help you today?

Can we get the replacement mushroon knob on the 9001KR16 E-stop?

Issue:
Is the mushroom knob replaceable on the 9001KR16 turn to release E-stop?


Product line:
30 mm Push Buttons


Environment:
Type K Heavy Duty Operators


Resolution:
No, the mushroom knob is not available as a replacement part, they will need to replace the 9001KR16 E-stop.

Schneider Electric Canada

Attachment(s)
9001KR16_document.pdf [214.13 KB]