Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can a selector switch be added to control ERMS on an MTZ Masterpact circuit breaker?
Issue:
Is there a way to use a physical switch to on/off ERMS, like in the case of Masterpact NT/NW?

Product Line:
Circuit Breakers

Resolution:
To control ERMS with a physical switch as was done with Masterpact NT, NW, and Powerpact, see ESM Switch Module.docx attached below.
First, you must have an MTZ breaker with the ERMS digital module installed, catalog number LV850009.
Second, you must have the ESM module installed. The breaker can be ordered from the factory with this module installed, or it can be field installed by Services. Instructions are attached.
Customer supplies the external switch and indicator light if desired.

NOTE:  The ESM module is not compatible with the M2C contacts.  Both cannot be installed.

Schneider Electric Canada

Attachment(s)
MTZ ESM ERMS Switch Module installation instructions PHA58571-00_HD.pdf [17.42 MB]
ESM Switch Module.pdf [140.34 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings