Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there an X80 backplane spacing requirement?

Issue
Will be mounting Modicon M340 or M580 backplanes and want to ensure proper spacing for cooling and air circulation.

Product line
Modicon X80, Modicon M340, Modicon M580

Resolution
Attached is the Modicon X80 Racks and Power Supplies Hardware Reference Manual. On pages 35 & 36, the optimal spacing is discussed.

Schneider Electric Canada

Attachment(s)
Modicon X80 Racks and Power Supplies Hardware Reference Manual 2023.pdf [7.8 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings