Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference is between a MN-S3-2 and a MN-S3-500 sensors ?
Issue:
Can the MN-S3-2 and MN-S3-500 sensors be used with I/A controllers?

Product:
I/A Sensors

Environment:
Selection

Cause:
Product Features

Resolution:
The MN-S3-2 sensor is used with older I/A controllers, where as the new MN-S3-500 is used with newer I/A controllers . The MN-S3-2 should not be used with new controllers.
Note : When using the MN-S3-500 customer will also need cover part number DCQC-150-SE

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings