Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the handle force required to operate the handle of a Powerpact L frame circuit breaker?
Issue:
Force handle require for the Powerpact L frame circuit breaker.

Product Line:
Molded Case Circuit Breaker

Resolution:
OFF to ON: 47.2 lbs
ON to OFF: 41.8 lbs
TRIPPED to OFF: 59.8 lbs

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings