Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Unity Pro or Control Expert DFB pin usage evaluation
Issue
Looking for a function that will report whether a DFB input pin is connected or linked to a Variable.

Product line
Control Expert, Unity Pro

Resolution
The IS_PAR_CON block is a function used in DFB code to know if an input parameter (pin) or an input/output parameter (pin) is connected or linked to a variable when you use an instance of the DFB.

NOTE: This function is only usable inside a DFB. It is not permitted to be used outside of DFB code.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings