Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do the Powerpact B-frame breakers have a fungus treatment option?
Issue:
Is there an option for fungus treatment to be added on the B-frame breakers?

Product Line:
Molded Case Circuit Breakers

Resolution:
The Powerpact B-frame breakers are made with fungus resistant materials, so no additional fungus treatment is needed to make them resistant to fungus growth.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings