Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can Micrologic Ammeter trip units be used in MDGF modified differential ground fault systems?
Issue:
Which Micrologic trip units can be used for SGR source ground return and for MDGF systems?

Product Line:
Circuit Breakers

Resolution:
Yes, Ammeter trip unit type 6.0A can be used in MDGF and SGR ground fault systems, as can the 6.0P and 6.0H. See bulletin link below for documentation.

0613DB9905

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings