How can we help you today?

Which ULP cord do you need to connect the BCM in a breaker to a communication module?

Product Line:
Circuit breakers

Resolution:
You need a circuit breaker ULP cord to connect a BCM module to one of the communication modules.
It has bare wires for screw terminals on the breaker end and an RJ45 plug on the other.  Choose one of the following:

L     =     0.35 m (1.15 ft.)     LV434195
L     =     1.3 m (4.27 ft.)     LV434196
L     =     3 m (9.24 ft.)     LV434197
L     =     5 m (16.40 ft.)     LV434198