Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you apply a standard rated breaker at 100% of its rating if it is set to less than 80% of its maximum rating or sensor size?
Issue:
Is it OK to use an 80% rated breaker at 100% if set to less than 80% of its max. rating?

Product Line:
Circuit Breakers

Resolution:
No, the breaker is not labeled for 100% and doing so would be a violation of its UL listing

This question is not addressed directly in the NEC or UL, but it is addressed by the application statements and guidelines for standard and 100% rated breakers. They do not allow 100% application for any breakers but those so marked. For reference, please see the attachment and NEC 210.20(A)  and NEC 215.3.

Note that 100% marking is required only for continuous application at over 80% of the breaker rating (3 hours or more). Shorter periods of operation up to 100% of the breakers rating are allowed.

Example:
A standard rated 600A Powerpact L frame breaker (not labeled for 100%) set at 400A (less than 80% of 600A) could NOT be applied as if it were rated for 100%.
Set at 400A, this breaker would have a maximum continuous current rating of 400 x 80% = 320A.

Schneider Electric Canada

Attachment(s)
100% Rated 0600DB0702.pdf [67.63 KB]
Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings