Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are Normally Closed Power Contacts Available with Class 8903 Type S Lighting Contactors?
Issue:
Multipole lighting contactor needs to have normally closed (NC) contacts

Product Line:
NEMA Type S Lighting Contactors

Environment:
NEMA Contactors and Starters

Resolution:
The standard device is equipped with normally open power poles only, however there are provisions for factory installation or field installable 30 amp or 60 amp normally closed power pole adders (2 maximum).

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings