Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: What type of hardware is needed to install a breaker in an I-Line® panel?
Issue:
How are I-line breaker mounted in I-line panels and what equipment is needed?

Product Line:
Circuit Breakers

Resolution:
The I-Line® breakers plug on to the bus stack and have a mounting foot on the back of the breaker that bolts the breaker to the mounting pan. A screwdriver is needed to leverage the breaker onto the bus and to tighten the mounting screw. See the video below for more information on how to mount them.








Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings